Nexperia
Nexperia, headquartered in the Netherlands, is a global semiconductor company with a rich European history and over 12,500 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
Refer to the Resources & Support tab for the 2025 Product Selection Guide that presents Nexperia’s “Essential Semiconductor” portfolio of discrete, ESD, MOSFET, GaN FET, analog, and logic ICs.
Sản phẩm nổi bật theo Nexperia
NEX92x30-Q100 Dual-Channel Antenna LDO Regulators
Operate over a wide voltage range from 4V to 40V (45V load-dump protection).
NPS7601 Single-Channel Low IQ Load Switch
A regulated forward-drop load switch with always-on, true reverse current blocking capabilities.
Bảng đánh giá công tắc tải NEVB-NPS7601
Test the performance of the NPS7601, a low-loss integrated load switch, in different applications.